i.MX28 Linux fails out of the box

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 Linux fails out of the box

937 Views
mmaaxx
Contributor III

Hello, I just started working with i.MX28 + LCD module. It has 2 SD cards: Windows and Linux. 

I tried Windows - worked just fine. However, Linux SD card don't start graphics, here is what it says:

 

Setting the hostname to freescaleMounting filesystemsEXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22844EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22844EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22844ln: /etc/mtab: Input/output errormount: mounting usbfs on /proc/bus/usb failed: No such file or directoryStarting inetd:EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22974Starting the dropbear ssh server:EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22975EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22977EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22977EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22845EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22845EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22977Failed to start message bus: Failed to bind socket "/usr/var/run/dbus/system_bus_socket": Input/output errorEXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22843D-Bus per-session daemon address is: unix:abstract=/tmp/dbus-8HD7zZ9Ocq,guid=f34f28ad28345166c1651c7f00000302EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 31422EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 239EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 239EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22845gtk: creating gdk-pixbuf.loaderspango: creating module liststarting pid 2165, tty '': '/sbin/getty -L ttyAM0 115200 vt100'EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 31422EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 31422
Fatal server error:Can't read lock file /tmp/.X0-lock

arm-none-linux-gnueabi-gcc (GCC) 4.1.2root filesystem built on Fri, 10 Sep 2010 12:31:16 -0600Freescale Semiconductor, Inc.
freescale login: EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22843matchbox-panel: failed to open dEXT2-fs error (device mmcblk0p3): ext2_lookup: isplaydeleted inode referenced: 22843matchbox-desktop: unable to open display !EXT2-fs error (device mmcblk0p3): ext2_lookup: deleted inode referenced: 22843matchbox: can't open display! check your DISPLAY variable.
arm-none-linux-gnueabi-gcc (GCC) 4.1.2root filesystem built on Fri, 10 Sep 2010 12:31:16 -0600Freescale Semiconductor, Inc.
freescale login:

 

Can anybody help? 

This is totally "out of the box" experience, should it work? at least out of the box? :(

Tags (1)
0 Kudos
Reply
1 Reply

631 Views
daiane_angolini
NXP Employee
NXP Employee

Can´t you see Tux?

 

You got prompt, everything must be fine.

0 Kudos
Reply