Hi,
I have an imx27ads board which got some problems when I turned on the board
as below:
++... Read from 0x07ee0000-0x07f00000 at 0xc1fe0000: .
... Read from 0x07ed3000-0x07ed4000 at 0xc1fff000: .
PMIC ID: 0x0000009b [Rev: 3.3]
Ethernet FEC MAC address: is not set
Board Type: EVB [rev A] (external UART doesn't work)
Clock input: 27 MHz
Booting from [NOR flash]
[Warning] FEC not connect right PHY: ID=fc03fc
FEC: [ HALF_DUPLEX ] [ connected ] [ 10M bps ]:
WARNING[can_send]: MXC_FEC is busy for transmittinig
WARNING[can_send]: MXC_FEC is busy for transmittinig
WARNING[can_send]: MXC_FEC is busy for transmittinig
Does anyone has ideas?
thanks a lot.
Elren