Hi,
I am preparing an USB driver for a board with iMX257 chipset.
I can read the register default values for OTG registers. But the Host1 registers are not in default values. All the values are read as Zero. Writing on those offset (0x0200 - 0x03A8) is also not reflecting. Whereas it is found that Host2 registers are in default values (though Host2 is not routed out).
I have set the hclk_usbotg clock. I wonder if any other clock setting is required for this or there may be some other setting. Is anyone having any idea? According to my understanding the usb_clk is enabled by default (Reason: By default usb_clk uses UPLL output as reference clock and UPLL is enabled by default).
I am stuck in the development.
Thanks in advance.
Regards,
Sayan Mukherjee
Hi igor,
Thanks for the file. But could you please spend a bit time in the following with YES or NO:
According to my understanding
where base address is 0x53FF4000.
According to the reference manual, there is no mention of Host2. But if we work using Host2
There exist stack of two USB ports.
From NXP support I got a reply that Host2 is non-functional in iMX257.
Regards,
Sayan
Hi Sayan
right.
0x400 can be found in ltib linux sources: linux/arch/arm/plat-mxc/include/mach/arc_otg.h
Board Support Packages (4)
Linux 2.6.31 Source Code Files 2009.12 Release support i.MX23, i.MX25, i.MX51. (REV 2009.12)
http://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-processors/i.mx25-product-developm...
Best regards
igor
Hi igor,
I did not find linux/arch/arm/plat-mxc/include/mach/arc_otg.h file in the "Linux 2.6.31 Source Code Files 2009.12 Release support i.MX23, i.MX25, i.MX51. (REV 2009.12)".
According to my understanding
where base address is 0x53FF4000.
According to the reference manual, there is no mention of Host2. But if we work using Host2
There exist stack of two USB ports.
From NXP support I got a reply that Host2 is non-functional in iMX257.
Regards,
Sayan
Hi Sayan
you are right, i.MX25 has only Host 2 registers under 0x400. There are
two on-chip USB ports with PHY, please check i.MX25 datasheet
Table 2. i.MX25 Parts Functional Differences
http://www.freescale.com/files/dsp/doc/data_sheet/IMX25CEC.pdf
High Speed USB OTG with HS PHY
High Speed USB Host with FS PHY
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Thanks for your reply.
This document is for iMX28. But I am working in iMX257.
Moreover, I have to work with the Host core. As only one Host core is routed out i.e the Host1 core, so I need to work with theregisters from offset 0x0200. Is this not feasible? I mean is there some special settings needed?
Regards,
Sayan
Hi Sayan
below correct link
http://www.freescale.com/files/dsp/doc/data_sheet/IMX25CEC.pdf
i.MX25 has only Host 2 registers under 0x400.
Also please check Table 4-18. i.MX25 Detailed Pin Muxing
i.MX25 Reference Manual
http://www.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf
Best regards
igor
Hi igor,
Thanks.
Do you mean to say that Host2 under 0x0400 is the only Host core available in iMX257? There is no mention of 0x0400 offset in the reference manual. There is only mention of 0x0200 for Host1. I am confused.
Regards,
Sayan