i.MX 8M Plus and eMMC(SDINBDG4-8G)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus and eMMC(SDINBDG4-8G)

754 Views
www1519
Contributor III

Hi! NXP Engineer

In my design,IMX8M Plus + eMMC(SDINBDG4-8G) is used.

the schematic is refer to NXP development kit.

eMMC’s PS is from PCA9450C.

But, when use uuu in USB Serial Download mode, download image to eMMC, failed.

and, the  first line of uuu the screen is 100%, then the second line is flashed, and uuu is closed.

Only one  board (others is ok)has error as shown in the following capture.

PCA9450C votage is normal.

By the way,the total of two batches of PCBs were produced, with one PCB in each batch indicating this phenomenon.

Pls help to resolute this. Thanks.

 

0 Kudos
Reply
4 Replies

678 Views
www1519
Contributor III

 

Hi! @riteshmpatel 

Capture as below. confirm,pls. Thanks a lot.

www1519_3-1693388718547.png

 

www1519_2-1693388678543.png

Best Reagrds.

 

 

 

0 Kudos
Reply

671 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @www1519,

Thanks for the captures.

While flashing in the USB Serial Download mode, are there any logs on the UART debug console?

If yes, could you please share that?

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

717 Views
www1519
Contributor III

Hi @riteshmpatel 

as below,confirm pls.

www1519_0-1693314153309.png

Best regards

 

0 Kudos
Reply

727 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @www1519,

I hope you are doing well.

I cannot see the capture of the error faced. Could you please attach the capture of the error?

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply