Hello, i would like to know if there is a possibility for decoding a H264 stream in gstreamer with the plugin vpudec (hardware decoder) in low latency on the i.MX 8M?
So in this posts (https://community.nxp.com/thread/304322) (https://community.nxp.com/thread/310455) it is possible on the i.MX 6 processor. Is this also possible for the i.MX 8M processor? There is this option "ReorderEnable" in imx-vpuwrap (disables buffer) that is not exposed to the gstreamer vpudec element properties. Does someone know if it is possible and how to disable the ReorderEnable option in imx-vpuwrap on the i.MX 8M?
The platform is an embedded system with an Yocto 2.5 (sumo) BSP.
In the working folder of the imx-vpuwrap recipe there are the files vpu_wrapper.c and vpu_wrapper_hantro.c. Could i disable ReorderEnable there an do a bitbake to take effect on the low latency decoding or what are the steps needed to alter the api or set parameters for the vpu wrapper (imx-vpuwrap)?
Regards
andy