i.MX 6SoloX missing NVCC_DRAM/_2P5 max currents

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6SoloX missing NVCC_DRAM/_2P5 max currents

675 Views
cmh
Contributor II

Hi

In the latest i.MX 6SoloX datasheet, the info for max supply currents of NVCC_DRAM and NVCC_DRAM_2P5 are missing. So what they will be if paring with single die LPDDR2 (800Mbps)?

Thanks!

Labels (1)
0 Kudos
Reply
2 Replies

561 Views
igorpadykov
NXP Employee
NXP Employee

Hi Changming

appnote for power consumption will be released soon, so far

one can use AN4580 i.MX 6SoloLite Power Consumption and

IMX6SLCEC  max. currents as they are similar to i.MX 6SoloLite.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

561 Views
cmh
Contributor II

Hi igor,

Appreciated the information! Worst use case defined in the app note AN4580 is audio playback, and the combined current (MPU+memory) is 8.5mA, which is quite low. Do you have other use cases that could exercise memory more? Want to get an idea on the max current or typ current during heavy use of the memory.

Thanks!

0 Kudos
Reply