Hai All,
m currently studying i.MX28 EVK for a project in a company and they provided me with this EVK. Can any one suggest an IDE supprting this freescale processor and also few applications( SAMPLE CODES) to try in it..? as part of my studies i need to come up with simulations as final output... its been a very long time i have been searching out for all this and seems to be quite difficult..
已解决! 转到解答。
Good day Yuri,
Just a heads up in that the IAR sample code for the i.MX28 is for a dev kit that is non existent... or maybe a very early/preliminary version of the dev kit that Freescale now offers. The biggest difference is that the one referenced in the IAR tools has completely different DDR and so you have to modify the project's DDR initialization routine. This in itself is not too difficult, as one can look to the OBDS code for the correct DDR initialization.
Cheers,
Sam
Hai all,
Thanks alot for all your replies.... I got my application confirmed for Mini Project.... Its to read values from a temperature sensor(LM75B) and to store in DDR2 memory and display the results through UART to PC.. The communication between the processor and LM75B is through I2C....!!... I
M totally new to the processor and now i have collected a lot datasheets related to each ...
I planning to write C code in IAR for each Module.... But i feel the programs i collected seems to be not supported in IAR .....!!:smileyconfused:
So my doubt is do i have to change the IDE (maybe Eclipse)..??
i have no idea how to get program for temperature sensor using I2C and run in i.MX processor
since i have to store in DDR2 memory....??:smileysad:....
does the DDR2 test code in the OBDS package be helpful for this application.../?
please i badly need help.. as am stuck.... no idea how to proceed...?/:smileyplain:..
ELINA...!!
Hi Elina,
I have the attached ADC test. It's very simple, it just takes samples of the different ADC channels and displays the results through the UART interface. You can flash it into an SD card and boot from it. I haven't run it through JTAG, but I think you should be able to do so with the axf image.
Hope this helps!
Best regards.
Jorge.
1.
At least as first step one can use Code Sourcery GNU toolchain (free Lite edition)
http://www.mentor.com/embedded-software/sourcery-tools/sourcery-codebench/editions/lite-edition/
If advantages of free Eclipse open-source Integrated Development Environment
(IDE) are needed, there is relevant plugin for ARM.
http://www.eclipse.org/downloads/download.php?file=/technology/epp/downloads/release
http://sourceforge.net/projects/gnuarmeclipse/
Also You may apply to IAR Workbanch - KickStart editon (size-limited evaluation license).
It contains example for i.MX28 too.
https://www.iar.com/Service-Center/Downloads/
2.
As code examples so called OBDS package may be useful.
https://www.freescale.com/webapp/Download?colCode=IMX_OBDS&appType=license&location=null
Good day Yuri,
Just a heads up in that the IAR sample code for the i.MX28 is for a dev kit that is non existent... or maybe a very early/preliminary version of the dev kit that Freescale now offers. The biggest difference is that the one referenced in the IAR tools has completely different DDR and so you have to modify the project's DDR initialization routine. This in itself is not too difficult, as one can look to the OBDS code for the correct DDR initialization.
Cheers,
Sam
Ur suggestions and links were so helpful in taking me forward..... now i chose IAR EWM for ARM...
Some applications that i could try out i got.....
Can u help me out how to configure ADC And UART in i.MX28 EVK....
there are a lot of registers related to these .. seems to be quite tuff and confusing ..:smileysad:
Any links or pdf's related to this.... pls pls forward it .... it would be helpful...!
Hai,,
i tried to configure internal ADC as ma mini project.... but since its a module wtihin the EVK... ma topic got rejected wen it was presented....:smileyshocked:... it was to to display the user key pressed in the EVK through the ADC and show the status in PC thro UART..... !!!
Now i really need an application to try in this i.MX28 EVK for mini project...other than internal Modules (OBDS package TEST)...
please can u help me out... something like..External memory interfacing with the EVK (perform some operations internally) and finally display the output through UART to LCD/PC...!!!