My project will use the watchdog in imx8 m40/
In code i test a situation---trigger the watchdog, but the whole system hangs on include linux of A core。
By reading the scfw_port.pdf, there is a way to use watchdog correctly that is to modify the scfw to create the partition for m40 watchdog.
But the scfw operation is dangerous, so afraid to
Hi Eric
I am afraid it is not possible as all resource management is handled by SCU using
SCFW APIs. On link below there is example for moving FlexCAN resources to A cores partition:
System Controller Firmware 101 - Resource management service
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------