how to use ov 5642

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use ov 5642

746件の閲覧回数
marshall123
Contributor II

Dear community:

hello, i have an ov5642 module using parallel connector ,one i.mx6qp sabre SD board and an environment running yocto project. how can i use this module on board? should i change the kernel or just type commands in board command line or write my code and cross compile it then run on the board?

Do you have a guide or some documents? sorry for the stupid question but I really donno how to continue.

thank you!

0 件の賞賛
1 返信

551件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please check sect.19.2 OV5642 Using parallel interface attached Linux Manual

and useful links
https://community.nxp.com/thread/329673
https://boundarydevices.com/ov5642-auto-focus-on-i-mx6/

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛