how to enable the qca wifi in imx8mq evk of android 10.0-1.0.0
our device is use the qca 6174 wifi in hardware,which was supported in android P-2.0.0-GA,and we want to upgrade to the latest android version android 10.0-1.0.0. But the android 10.0-1.0.0 use bcm wifi.
How to enable the qca 6174 on android 10.0-1.0.0
Hi zhulin
one can try latest qualcomm patches :
qcacld-2.0 - Unnamed repository
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor
I find in imx8mm use the QCA9377 and the interface is sdio , but my board is use the QCA6174A which use the pcie. when I insmod the wlan.ko, it shows as below:
[ 4709.296243] wlan: loading driver v4.5.24.4
[ 4709.302185] ath_hif_sdio: HIF (Atheros/multi-bss)
[ 4714.328552] AR6000: Unregistering with the bus driver
How to disable the sdio and change to pcie.