cluster display not working in i.MX8QM using LVDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cluster display not working in i.MX8QM using LVDS

1,323 Views
vishnudpai
Contributor II

Hi All,

I am currently working with android automotive build: mek_8q_car. I am trying to connect two displays using LVDS0_CH0 and LVDS1_CH1. I am connecting both the displays using LVDS-to-HDMI adapter. According to Android user guide, it states that one display will show the car launcher and other display will show the instrument cluster. But I am only seeing car launcher in one display and other display does not show anything(black screen).

Do I need to make any configuration changes?

My requirement: I need two displays simultaneously: One showing the car launcher and other showing the instrument cluster.

0 Kudos
Reply
3 Replies

1,274 Views
vishnudpai
Contributor II

Hi Bio_TICFSL,

Thanks for your reply, I haven't created any dts file for my own display because I thought multiple display was set to default in the build. In the android user guide it says only to connect the two displays with sas cable to LVDS 0 and 1.

vishnudpai_0-1686112499275.png

1.Do we need to create our own dts file for my display, if yes, then do you have any example dts file to take reference? . 

2.what command should I give in the uboot console for getting multiple displays?

3.Is there any other modification needed?

(btw I am not using demo images. I have build the source in my system and then flashing)

0 Kudos
Reply

1,208 Views
vishnudpai
Contributor II

Hi all,

Can anyone help me with this issue?.

0 Kudos
Reply

1,293 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you already have the dtb of your display running, then you need modification in uboot console.

 

Regards

0 Kudos
Reply