how to enable the qca wifi in imx8mq evk of android 10.0-1.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to enable the qca wifi in imx8mq evk of android 10.0-1.0.0

1,622件の閲覧回数
94393400
Contributor III

how to enable the qca wifi in imx8mq evk of android 10.0-1.0.0

our device is use the qca 6174 wifi in hardware,which was supported in android P-2.0.0-GA,and we want to upgrade to the latest android version android 10.0-1.0.0.  But the  android 10.0-1.0.0 use bcm wifi.

  How to enable the qca 6174 on  android 10.0-1.0.0

ラベル(1)
0 件の賞賛
5 返答(返信)

1,516件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhulin

one can try latest qualcomm patches :

qcacld-2.0 - Unnamed repository 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,516件の閲覧回数
94393400
Contributor III

Hi igor

        I find  in imx8mm use the QCA9377 and the interface is sdio , but my board is use the QCA6174A which use the pcie. when I insmod the wlan.ko, it shows as below:

[ 4709.296243] wlan: loading driver v4.5.24.4
[ 4709.302185] ath_hif_sdio: HIF (Atheros/multi-bss)
[ 4714.328552] AR6000: Unregistering with the bus driver

How to disable the sdio and change to pcie.

0 件の賞賛

555件の閲覧回数
Udhay_
Contributor III

hi how did you enable sdio in qca9377 in imx8mm?

0 件の賞賛

1,516件の閲覧回数
94393400
Contributor III

How about the android side, not use the qcom service now?

0 件の賞賛

1,516件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

qca module is supported for i.MX8M Mini EVK board so you

can try to port changes from that release.

Best regards
igor

0 件の賞賛