how can i Download the Freescale i.MX23-EVK BSP??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how can i Download the Freescale i.MX23-EVK BSP??

1,203 次查看
stevenshan
Contributor II

hello,

how can i Download the Freescale i.MX23-EVK BSP??who can help me?

标签 (2)
0 项奖励
回复
4 回复数

1,058 次查看
stevenshan
Contributor II

Thanks igor,  is  WCE600_10.05.02_SDK.msi  include bsp of I.mx23 EVK ? i  need to install WCE600_10.05.02_SDK.msi,and then bsp will be installed, ringt?

0 项奖励
回复

1,058 次查看
igorpadykov
NXP Employee
NXP Employee

yes it is for I.mx23 EVK.

~igor

1,058 次查看
igorpadykov
NXP Employee
NXP Employee

Hi steven

i.MX233 Processors|PMU|Freescale

WCE600_10.05.00_SDK : 2010.05 Windows Embedded CE 6.0 Source Code.

Size (K): 23635 Format: zip Rev #: 2010.05 Modified: 6/19/2010


Best regards

igor

1,058 次查看
erikvandenbroek
Contributor I

AFAIK U can use the latest wince600 package. It should contain the iMX233 bsp

U can download it here

i.MX515 Processors|Advanced HMI|Freescale

(Assuming it's the wince60 BSP U are looking for)

0 项奖励
回复