Thanks igor, is WCE600_10.05.02_SDK.msi include bsp of I.mx23 EVK ? i need to install WCE600_10.05.02_SDK.msi,and then bsp will be installed, ringt?
yes it is for I.mx23 EVK.
~igor
Hi steven
i.MX233 Processors|PMU|Freescale
WCE600_10.05.00_SDK : 2010.05 Windows Embedded CE 6.0 Source Code.
Size (K): 23635 Format: zip Rev #: 2010.05 Modified: 6/19/2010
Best regards
igor
AFAIK U can use the latest wince600 package. It should contain the iMX233 bsp
U can download it here
i.MX515 Processors|Advanced HMI|Freescale
(Assuming it's the wince60 BSP U are looking for)