gstreamer version in fsl-image-qt5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gstreamer version in fsl-image-qt5

2,094 Views
rans
Senior Contributor I

Hello,

We recently started working with fsl-image-qt5 (but using adlink layer lec-imx)

We found out that gstreamer version is 1.6.
We need to use more update version (1.8)

I am not sure yet if it is related to lec-imx layer or to fsl-image-qt5 layer.

Does fsl-image-qt5 force 1.6 version for gstreamer ?

Regards,

Ran

2 Replies

635 Views
igorpadykov
NXP Employee
NXP Employee

Hi ran

GStreamer version in NXP Linux 4.9.11_1.0.0 BSP described on below link is 1.10.4

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

It is described in Release Notes included in doc package:

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

635 Views
rans
Senior Contributor I

Hi Igor,

Thank you for the information.

We need to add openvivoe into yocto.

It is supported in yocto (meta-openvivoe/recipes-multimedia at master · Openwide-Ingenierie/meta-openvivoe · GitHub ), but trying to add it to lec-imx6 (adlink based on fsl-image-qt5), it returns error about mismatch gstreamer version.

gstreamer1.0-plugins-good_1.8.2.bbappend

It seems that lec-imx6 is using gstreamer 1.6.

Do you have any idea how we can resolve this issue ? Does moving to latest fsl-image-qt5 release can resolve this issue (I see it is using gstreamer 1.12, so there might still be some issues ? I'm not sure)

Thank you,

Ran

0 Kudos
Reply