hi, I'm pretty new in embedded world. I've got a evk board on my hand with a cpu of type "imx8m". I've checked out all the files in mcuexpresso version 2.7 and found no files named like "fsl_fec" "fsl_enet" or any examples implement phy in cm4 world.
my question is "is it possible for phy working on m4 core" if so, is there any brief tutorial I can follow
best regards
pan
已解决! 转到解答。
Referring to the R.M, we can see that most peripherals are shared among both the core A7 and M4. RDC will be the one managing the access of peripherals between both the cores.
Yes, it is possible to use Ethernet on M4 core.However, the current SDK does not have support for Ethernet driver.
Regards,
Kunal
Referring to the R.M, we can see that most peripherals are shared among both the core A7 and M4. RDC will be the one managing the access of peripherals between both the cores.
Yes, it is possible to use Ethernet on M4 core.However, the current SDK does not have support for Ethernet driver.
Regards,
Kunal
Hello,
could you please add a bit of information or some kind of note here, that could be helpful to anyone going through this kind of use case?
We need the same thing, ethercat over ethernet on M4 core. Not necessary on A53.
Thanks in advance!
Stefano
Glad you have developed the ethernet driver. Thanks for letting us know. Have you taken the ethernet driver reference from the linux kernel source and ported the same on FreeRTOS? Can you please add an information or some kind of note here, that could be helpful to anyone going through this kind of use case?
Regards,
Kunal
Hi,
I ran into a other problem. after I build the EtherCAT stack on M4 core and the motion control app on Linux side and try to combine these two together. It seems thad I can't boot these two together. The problem seems caused by two core touches the ENET while booting together. So I tried to use the RDC(kRDC_Periph_ENET1) to lock the ENET and remove the device tree node which matches "*fec*" or "*enet*" and still the linux side touches the enet register and caused ----"Synchronous Abort" handler, esr 0x96000210"---- all the time.
Could you give me some hint about it ?
Thank you so much
Hello xiang,
You can not use the same Ethernet interface with different OSes.
You need to drive Ethernet from one OS and access it from another using something like messaging unit.
However it is not a good idea. This way you loose speed and realtime.
If you mean i.MX8 processor not i.MX8M please note that it has 2 Ethernet interfaces.
So yo can use one with RTOS runing on M4 core and another with Linux runing on A ones.
Regards
thank you.
sorry for not making it clear.
I'm not going to share the phy with m4 core. I just want it work on m4 but not on CortexA53 core.
can I just delete it from the device tree and use it on m4 core side?
beat regards
pan