enable CAN in i.MX6SoloX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

enable CAN in i.MX6SoloX

1,285件の閲覧回数
jibin1246
Contributor II

How to enable CAN in i.MX6SoloX ?

0 件の賞賛
返信
1 返信

1,100件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The Linux BSP already includes FlexCAN drivers for i.MX6SX (mounted as a network interface). In order to check the driver overview, hardware and software operation, source code structure and menu configuration options please refer to Chapter 37 “FlexCAN Driver” of the “i.MX Linux® Reference Manual” document (attached).

It may be also required to change the Device Tree file, as there could be some pin conflicts. Please take a look at Table 10 “Supported features” of the “i.MX Linux® Release Notes” document (also attached).

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------