Hello,
You may look at the following:
https://community.nxp.com/message/995816
Also, perhaps it makes sense to try new SDK, that should be issued soon.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have downloaded newest version of SDK.
In emwin_gui_demo example, there is sdram_debug mode example code.
But it can't used for MP. only flexspi_nor or xip mode can be MP.
But both these of mode can't work on emwin_gui_demo.
I have done bubble example with flexspi_nor and xip mode. Both two mode have same behavior as it perform in sdram_debug.
Could you deliver the workable emwin_gui_demo example code with flexspi_nor or xip mode