emmc v5.1问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emmc v5.1问题

Jump to solution
4,768 Views
zengzhaoping
Contributor II

现在项目采用了东芝MMCA Version 5.1 ,内核的mmc驱动支持出现些问题,log如下

[    3.865587] Galcore version 5.0.11.25762

[    3.960991] mmc3: unrecognised EXT_CSD revision 8

[    3.965803] mmc3: error -22 whilst initialising MMC card

现在采取的解决方法是mmc.c if (card->ext_csd.rev > 6)  改成 > 8 但这应该不是好的解决方案

我们用的时候imx6q +android4.4.3 +linux3.10.53,有没有更好的解决方案

Labels (4)
0 Kudos
Reply
1 Solution
2,995 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You do not need to modify other code. The emmc v4.5 is default supported and here we change the ext_csd.rev to make the emmc v5.1 work on emmc v4.5 mode. It's OK and can work well.

Have a great day,

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
7 Replies
2,995 Views
ningli
Contributor III

你好,我也在使用东芝的emmc ver5.1 芯片 我按你说的方法修改了代码,但是还是不能启动,目前报错是

mmc0: starting CMD6 arg 03b34b01 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD6): -110, retrying...

sdhci [sdhci_irq()]: *** mmc0 got interrupt:

在mmc_switch  part_config 的设置为0x4时返回 超时!请问你遇到过这个问题吗,能否留个联系方式 共享下你们的emmc驱动

我的邮箱ramon20082001@163.com

0 Kudos
Reply
2,995 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ning,

You can refer to EMMC 5.0 and EMMC 5.1 work on i.MX6  in our community.

Have a nice day

Dan

0 Kudos
Reply
2,995 Views
ningli
Contributor III

这个部分已经改了 ,问题好像跟这个没关系

0 Kudos
Reply
2,995 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

If you do above modify and it can not work. First you can check the value of ext_csd.rev. And then check the BOOT_CFG[7:5] emmc setting 010 8bit.

Best Regards

Dan

0 Kudos
Reply
2,995 Views
zengzhaoping
Contributor II

感谢回复:

mmc.c if (card->ext_csd.rev > 6)  改成 > 8 可以工作正常的;

现在我的理解是我们的emmc芯片是emmc v5.1的 但是驱动支持的是emmc v4.5;

我想是不是可以修改驱动支持emmc v5.1 来提高emmc的读写速度。

0 Kudos
Reply
2,996 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You do not need to modify other code. The emmc v4.5 is default supported and here we change the ext_csd.rev to make the emmc v5.1 work on emmc v4.5 mode. It's OK and can work well.

Have a great day,

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,995 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

When you change the  mmc.c if (card->ext_csd.rev > 6)  to > 8 , can it work fine? By now in our side we use this method modify the value of card->ext_csd.rev to make the EMMC 4.4 above version work .
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply