drive strength

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

drive strength

1,344件の閲覧回数
geethar
Contributor II

How to change the drive strength of mobile DDR?

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,076件の閲覧回数
geethar
Contributor II

How can i access the mobile DDR mode register and extended mode register address?

How to set mode register in DDR?

0 件の賞賛
返信

1,076件の閲覧回数
geethar
Contributor II

part number for my micron mobile ddr is MT46H32M16LFBF-6 IT:C

0 件の賞賛
返信

1,076件の閲覧回数
Yuri
NXP Employee
NXP Employee

  According to the MT46H32M16LFBF  Datasheet, Extended Mode Register (EMR)

controls in particular drive strength. The EMR is programmed via the LOAD MODE REGISTER
command with BA0 = 0 and BA1 = 1. EMR bits 5,6,7 define memory drive strength.

< http://www.micron.com/~/media/Documents/Products/Data%20Sheet/DRAM/Mobile%20DRAM/Low-Power%20DRAM/LP... >



IMX23 provides EMR writing via setting bit field HW_DRAM_CTL38 [EMRS1_DATA] and

setting HW_DRAM_CTL09 [ WRITE_MODEREG ].

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,076件の閲覧回数
Yuri
NXP Employee
NXP Employee

What is modile DDR (part number, Datasheet) ?

0 件の賞賛
返信

1,076件の閲覧回数
Yuri
NXP Employee
NXP Employee

   Please use DDR Mode registers (Extended Mode Register) to configure DDR

Output Drive Strength during DDR initialization.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信