I'm building the custom yocto image for the iMX8m mini. It builds gstreamer-1.18.5.imx At first, I am seeing video4linux2 shared lib was installed in rootfs with default package configuration options as mentioned at gstreamer1.0-plugins-good_1.18.5.imx.bb The build succeeded.
But on the target board the $gst-inspect-1.0 | grep v4l2 only outputs 3 plugins:
I'm actually looking for below video decoder plugins as mentioned in i.MX8GStreamerUserGuide -
I don't have any of them and I don't really understand why it's not there whereas the yocto recipes have all succeeded.
Can anyone suggest something which I have to look for to fix this issue?
Thanks @Bio_TICFSL
I'm not seeing much of the difference between my machine configuration(attached commboard.zip) and machine conf in meta-freescale but still, I'm not getting those plugins in the final image. Do you suspect anything suspicious in the attached machine configurations that I need to take care so that I will get those plugins.
__PRESENT
Hello,
Yes, you have it, in yocto if you are building the full image, just $gst-inspect will give you the codecs you have.
Regards