burn fuses

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

burn fuses

1,280 Views
sapirbuz
Contributor IV

Hi,

How can we burn the fuses without an external flash on our board?

Can we use the internal ROM to do it?

sapirbuz_0-1679415733546.png

 

0 Kudos
Reply
8 Replies

1,262 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

On the i.MX8 and i.MX8x families the OTP memory is part of the security subsystem and is controlled by the SCU and SECO only. Please refer to this blog post about how users can read and write eFuses.

Understanding how to burn eFuses on i.MX8 and i.MX8x families.

Best regards.

0 Kudos
Reply

1,252 Views
sapirbuz
Contributor IV

Sorry, but i still don't understand if it is possible to burn fuses without an external flash, and how to do it in case it is possible

0 Kudos
Reply

1,244 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Yes, you can burn fuses internally using U-boot, once the board is flashed you can use U-boot commands to read/write efuses using the SCFW API functions that are specified on the blog that is on the past answer.

Best regards.

0 Kudos
Reply

1,240 Views
sapirbuz
Contributor IV

What do you mean by "when the board is flashed"?

0 Kudos
Reply

1,238 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It means that you have an image flashed on the board and it is able to boot.

Best regards.

0 Kudos
Reply

1,232 Views
sapirbuz
Contributor IV

If I have an image flashed on the board, it means that I have an external flash on the board, right?

But the external flash wasn't enabled (because we need to burn the fuses first) so it is like we don't have an external flash on the board.

How can we burn the fuses without an external flash on our board and we don't have an image flashed on the board?

0 Kudos
Reply

1,218 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Got it, it that case it is not possible, you need to flash the MPU to burn efuses.

Best regards. 

0 Kudos
Reply

1,198 Views
sapirbuz
Contributor IV

You are wrong.

It is possible using the LPSPI NOR/EEPROM.

After setting the "Boot Device" to "LPSPI NOR/EEPROM" , we succeed to burn the fuses.

0 Kudos
Reply