Hello NXP,
For one of our custom board having processor of i.mx6 series, currently, we are building all required images separately - u-boot, kernel, device tree and root fs. Now, we need .sdcard image to generate which has all the images in one file.
I have gone through the below links:
https://community.nxp.com/t5/i-MX-Processors/Yocto-stopped-building-sdcard-files/m-p/278555#M31585
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Guide-to-the-sdcard-format/ta-p/1107441
with this, we have below error:
"No IMAGE_CMD defined for IMAGE_FSTYPES entry 'sdcard' - possibly invalid type name or missing support class"
I have also checked below link:
https://community.nxp.com/t5/i-MX-Processors/Imx8qmmek-Sdcard-Image-Support/m-p/960091#M143290
But, I am not able to open Linux L4.14.98_2.0.0 Documentation mentioned.
I have checked below link also:
https://community.nxp.com/t5/i-MX-Processors/IMX6UL-EVKB-Image-building-issue/m-p/1019046
It says to change the SHELL. But this also does not resolve the issue.
Kindly guide me to generate the required .sdcard image successfully.
Thanks,
Pandurang
Hello,
Please try using the script fsl-setup-release.sh, this script sets up a directory and the configuration files for the specified machine and backend.
The syntaxis is as following:
Also, you may find all Linux BSP documentation here:
https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...
As for Documentation package for L4.14.98_2.2.0, you may download it from here:
https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga
Best regards,
Aldo.