avimux issue - gst_avi_mux_write_avix_index:<avimux0> No more room in superindex of stream 00db

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

avimux issue - gst_avi_mux_write_avix_index:<avimux0> No more room in superindex of stream 00db

1,606 Views
madstrum
Contributor III

Hi,

I am using GStreamer to do raw recording on imx6 using the following pipeline.

gst-launch -e tvsrc fps-n=25 ! queue2 max-size-buffers=1 max-size-bytes=0 max-size-time=0 ! 'video/x-raw-yuv, width=(int)720, height=(int)576, framerate=(fraction)25/1' ! avimux ! queue2 max-size-buffers=1 max-size-bytes=0 max-size-time=0 ! filesink location=output.avi --gst-debug-level=3

It runs fine for some time recording the avi until around the 35min mark gst debug gives me this.

avimux gstavimux.c:c:1540:gst_avi_mux_write_avix_index:<avimux0> No more room in superindex of stream 00db

The video then stops recording effectively even though gstreamer continues.

When I look at the video the frame count ends at the 35min mark.

How can I resolve this? Is this a bug in avimux?

0 Kudos
Reply
6 Replies

1,374 Views
igorpadykov
NXP Employee
NXP Employee

Hi mad

seems board has insufficient memory, in general it may be recommended

to try latest BSP which has gstreamer 1.4 supported

L3.14.28_1.0.0_iMX6QDLS_BUNDLE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,374 Views
madstrum
Contributor III

I just like to add : When I use vpuenc to encode it to H.264 before sending it to avimux, it runs ok.

ie. vpuenc codec=6 bitrate=1000000 ! avimux

0 Kudos
Reply

1,374 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

1,374 Views
madstrum
Contributor III

Hi,

So there isn't any resolution for this?

Does the drop cache method (from your link) really work?

My RAW recording with tvsrc always drops out around 35min - I can't be the only one who's experiencing this.

0 Kudos
Reply

1,374 Views
igorpadykov
NXP Employee
NXP Employee

please try with latest BSP

L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux

0 Kudos
Reply

1,374 Views
madstrum
Contributor III

Hi igor,

The board has 1GB of memory, is this not enough?

Is there a memory leak in this particular plugin?

0 Kudos
Reply