Hi,
I am using GStreamer to do raw recording on imx6 using the following pipeline.
gst-launch -e tvsrc fps-n=25 ! queue2 max-size-buffers=1 max-size-bytes=0 max-size-time=0 ! 'video/x-raw-yuv, width=(int)720, height=(int)576, framerate=(fraction)25/1' ! avimux ! queue2 max-size-buffers=1 max-size-bytes=0 max-size-time=0 ! filesink location=output.avi --gst-debug-level=3
It runs fine for some time recording the avi until around the 35min mark gst debug gives me this.
avimux gstavimux.c:c:1540:gst_avi_mux_write_avix_index:<avimux0> No more room in superindex of stream 00db
The video then stops recording effectively even though gstreamer continues.
When I look at the video the frame count ends at the 35min mark.
How can I resolve this? Is this a bug in avimux?
Hi mad
seems board has insufficient memory, in general it may be recommended
to try latest BSP which has gstreamer 1.4 supported
L3.14.28_1.0.0_iMX6QDLS_BUNDLE
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
So there isn't any resolution for this?
Does the drop cache method (from your link) really work?
My RAW recording with tvsrc always drops out around 35min - I can't be the only one who's experiencing this.
please try with latest BSP
L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux