Dear all
I download 5.10.72 nxp official release, and have following onnxruntime qa issue while imx-image-full build, need help, thank you.
I have tried 8mm and 8mp, imx-image-full always failed, and imx-image-multimedia can pass the build.
My build system is ubuntu 20.04.
ERROR: onnxruntime-1.8.2-r0 do_package_qa: QA Issue: /usr/lib/python3.9/site-packages/bin/onnxruntime_test contained in package onnxruntime requires /build/imx8mp/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot-native/usr/bin/nativepython3, but no providers found in RDEPENDS_onnxruntime? [file-rdeps]
ERROR: onnxruntime-1.8.2-r0 do_package_qa: QA run found fatal errors. Please consider fixing them.
ERROR: Logfile of failure stored in: /build/imx8mp/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/temp/log.do_package_qa.557189
ERROR: Task (/build/sources/meta-imx/meta-ml/recipes-libraries/onnxruntime/onnxruntime_1.8.2.bb:do_package_qa) failed with exit code '1
解決済! 解決策の投稿を見る。
Indeed this issue is fixed since 5.10.35-2.0.0 where the branch name is specified.
On 5.4.70-2.3.0 (and earlier than 5.10.35-2.0.0) you need to modify SRC_URI in the recipe:
SRC_URI = "git://github.com/onnx/onnx.git;branch=main"
Indeed this issue is fixed since 5.10.35-2.0.0 where the branch name is specified.
On 5.4.70-2.3.0 (and earlier than 5.10.35-2.0.0) you need to modify SRC_URI in the recipe:
SRC_URI = "git://github.com/onnx/onnx.git;branch=main"
When I build imx-image-full, some error occured!
fatal: unsafe repository ('....tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/build/pybind11/src/pybind11' is owned by someone else) | To add an exception for this directory, call: | | git config --global --add safe.directory ...../tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/build/pybind11/src/pybind11
I know I can use "git config --global --add safe.directory ...../tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/build/pybind11/src/pybind11" to fix it.
But I don't want do it when re-build by others, How can I fix the issue?
Best Regards
Qing
Did you get any resolution for this issue with pybind11?
i don't think so , due to he use new version already , please check here:
I download 5.10.72 nxp official release,
secondly , his error messae is not ( do_fetch )
WARNING: armnn-onnx-1.3.0-r0 do_fetch: Failed to fetch URL git://github.com/onnx/onnx.git, attempting MIRRORS if available
his error is this (do_package_qa)
ERROR: onnxruntime-1.8.2-r0 do_package_qa: QA Issue:
solved :
oh i studied this error careful ,you can re create a clean folder redo all sure OK
thank you all
Hi Joseph
I rebuild with 5.10.35 with successful, however I can't do it succesully with 5.10.72.
Could you help clarify in detail that "create a clean folder and redo OK"?
I have clean build several times with 5.10.72, QA Issue always occurred.
thank you!
oh then confirmed QA issues lah pls wait NXP solved it