Hi,
in newer kernels 5.4.x, the device tree structure is quite different and the nodes lsio_pwm0-7 are completely missing.
Porting them from previous 4.14.x seems to be quite tricky.
Do you have any sample implementation working for iMX8QM?
Thanks
Regards
Pier
Hi, have you find any solution ?
We are now facing the same problem, and we think we should now refer to the Low Power Clock Gate (lpcg_pwm[0-7]) taking example from imx8qxp. Neverless I can't understand the relation between lpcg_pwm and lsio_pwn (see memor map descriptio in attached pdf).
Bye
Giuseppe
Hi Joan,
We are using NXP Linux BSP Yocto Gatesgarth version now, the kernel is 5.10.9. and we need to enable LSIO PWM2 (IMX8QM_GPT1_COMPARE_LSIO_PWM2_OUT) but we also can't find any LSIO PWM0~7 definition or examples in freescale devicetree folder. In NXP Linux BSP 4.19.35, the related LSIO PWM definintion is in fsl-imx8qm-device.dtsi as below. Could you tell us where can we find a example or related definition about LSIO PWM0~7 for reference? Thanks~
fsl-imx8qm-device.dtsi in kernel_imx\arch\arm64\boot\dts\freescale
pwm0: pwm@5d000000 {
compatible = "fsl,imx8qm-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d000000 0 0x10000>;
clocks = <&clk IMX8QM_PWM0_IPG_MSTR_CLK>,
<&clk IMX8QM_PWM0_HF_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QM_PWM0_HF_CLK>;
assigned-clock-rates = <24000000>;
#pwm-cells = <2>;
power-domains = <&pd_lsio_pwm0>;
status = "disabled";
};
pwm1: pwm@5d010000 {
compatible = "fsl,imx8qm-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d010000 0 0x10000>;
clocks = <&clk IMX8QM_PWM1_IPG_MSTR_CLK>,
<&clk IMX8QM_PWM1_HF_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QM_PWM1_HF_CLK>;
assigned-clock-rates = <24000000>;
#pwm-cells = <2>;
power-domains = <&pd_lsio_pwm1>;
status = "disabled";
};
pwm2: pwm@5d020000 {
compatible = "fsl,imx8qm-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d020000 0 0x10000>;
clocks = <&clk IMX8QM_PWM2_IPG_MSTR_CLK>,
<&clk IMX8QM_PWM2_HF_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QM_PWM2_HF_CLK>;
assigned-clock-rates = <24000000>;
#pwm-cells = <2>;
power-domains = <&pd_lsio_pwm2>;
status = "disabled";
};
pwm3: pwm@5d030000 {
compatible = "fsl,imx8qm-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d030000 0 0x10000>;
clocks = <&clk IMX8QM_PWM3_IPG_MSTR_CLK>,
<&clk IMX8QM_PWM3_HF_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QM_PWM3_HF_CLK>;
assigned-clock-rates = <24000000>;
power-domains = <&pd_lsio_pwm3>;
#pwm-cells = <2>;
status = "disabled";
};
pwm4: pwm@5d040000 {
compatible = "fsl,imx8qm-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d040000 0 0x10000>;
clocks = <&clk IMX8QM_PWM4_IPG_MSTR_CLK>,
<&clk IMX8QM_PWM4_HF_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QM_PWM4_HF_CLK>;
assigned-clock-rates = <24000000>;
#pwm-cells = <2>;
power-domains = <&pd_lsio_pwm4>;
status = "disabled";
};
pwm5: pwm@5d050000 {
compatible = "fsl,imx8qm-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d050000 0 0x10000>;
clocks = <&clk IMX8QM_PWM5_IPG_MSTR_CLK>,
<&clk IMX8QM_PWM5_HF_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QM_PWM5_HF_CLK>;
assigned-clock-rates = <24000000>;
#pwm-cells = <2>;
power-domains = <&pd_lsio_pwm5>;
status = "disabled";
};
pwm6: pwm@5d060000 {
compatible = "fsl,imx8qm-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d060000 0 0x10000>;
clocks = <&clk IMX8QM_PWM6_IPG_MSTR_CLK>,
<&clk IMX8QM_PWM6_HF_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QM_PWM6_HF_CLK>;
assigned-clock-rates = <24000000>;
#pwm-cells = <2>;
power-domains = <&pd_lsio_pwm6>;
status = "disabled";
};
pwm7: pwm@5d070000 {
compatible = "fsl,imx8qm-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d070000 0 0x10000>;
clocks = <&clk IMX8QM_PWM7_IPG_MSTR_CLK>,
<&clk IMX8QM_PWM7_HF_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QM_PWM7_HF_CLK>;
assigned-clock-rates = <24000000>;
#pwm-cells = <2>;
power-domains = <&pd_lsio_pwm7>;
status = "disabled";
};
I also need a solution for this. There's a bunch of imx8qm-ss-*.dtsi files but no imx8qm-ss-pwm.dtsi, so the PWMs are not usable, and directly reusing the PWM definitions from the 4.14 kernels isn't possible because the clock definitions have also changed.
Here's a link to the PWM nodes from kernel 4.14: fsl-imx8qm-device.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel
Hi Joan,
in kernel 4.14, pwm are available starting from here
fsl-imx8qm-device.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel
The name was just pwmX, but were actually referring to LSIO area.
Please let me know if you need further details.
Thanks
Regards
Pier