YUV422 (UYVY) Camera support on Imx8m mini Android9.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

YUV422 (UYVY) Camera support on Imx8m mini Android9.0

1,264 Views
Andrew_yang
Contributor II

Hi,

I transplanted a camera with MIPI CSI interface on the IMX8 platform Android9.0, and the image output format of the camera is  UYVY(YUV422) ,1920*1080p. 

After debugging, I found that when I opened the camera preview, there was an image just opened, but the picture would get stuck immediately. The following error log message is prompted:

**************************************************************************
06-10 14:00:18.028 3111 3226 I FslCameraHAL: configureStreams:0: stream_config 0xf45ff500, num 2, streams 0xf4485008, mode 0
06-10 14:00:18.028 3111 3226 I FslCameraHAL: config 0, type 0, res 1920x1080, fmt 0x21, usage 0x3, maxbufs 1, priv 0xf44c3000, rotation 0
06-10 14:00:18.028 3111 3226 I FslCameraHAL: config 1, type 0, res 1920x1080, fmt 0x102, usage 0x100, maxbufs 2, priv 0xf44c30e0, rotation 0
06-10 14:00:18.029 4336 4407 D CAM_CommandExecutor: Executing command: com.android.camera.one.v2.commands.PreviewCommand@c383ecf END
06-10 14:00:18.030 3150 4400 D Camera3-Device: Set real time priority for request queue thread (tid 4400)
06-10 14:00:18.033 3116 3116 E gralloc : convertAndroidFormat invalid format:0x102
06-10 14:00:18.033 3116 3116 E display : checkFormat unsupported format:0x0
06-10 14:00:18.062 3150 4400 I display : open gpu gralloc module!
06-10 14:00:18.073 3111 3226 I display : open gpu gralloc module!
06-10 14:00:18.074 3111 3226 I FslCameraHAL: configure: w:1920, h:1080, sensor format:0x102, stream format:0x102, fps:30, num:3
06-10 14:00:18.074 3111 3200 I FslCameraHAL: onDeviceConfigureLocked
06-10 14:00:18.074 3111 3200 I FslCameraHAL: Width * Height 1920 x 1080 format UYVY, fps: 30
06-10 14:00:18.075 3116 3116 E gralloc : convertAndroidFormat invalid format:0x102
06-10 14:00:18.075 3116 3116 E display : checkFormat unsupported format:0x0
06-10 14:00:18.138 3111 3226 I FslCameraHAL: configure: w:1920, h:1080, sensor format:0x102, stream format:0x102, fps:30, num:3
06-10 14:00:18.138 3111 3200 I FslCameraHAL: onDeviceStartLocked
06-10 14:00:18.162 3140 3207 W SurfaceFlinger: Attempting to set client state on removed layer: Splash Screen com.android.camera2#0
06-10 14:00:18.162 3140 3207 W SurfaceFlinger: Attempting to destroy on removed layer: Splash Screen com.android.camera2#0
06-10 14:00:18.170 3111 3200 I FslCameraHAL: onDeviceStartLocked VIDIOC_QBUF phy:0x8f800000
06-10 14:00:18.170 3111 3200 I FslCameraHAL: onDeviceStartLocked VIDIOC_QBUF phy:0x8fc00000
06-10 14:00:18.170 3111 3200 I FslCameraHAL: onDeviceStartLocked VIDIOC_QBUF phy:0x90000000
06-10 14:00:18.197 4336 4336 V CAM_CaptureModule: AF status is state:INACTIVE
06-10 14:00:18.307 3111 3200 E : g2d_blitEx: Invalid dst planes[0] pointer=0x0 !
**************************************************************************

When the screen is stuck,The following log information appears:

**************************************************************************

06-10 14:00:41.063 3150 4400 E Camera3-Stream: getBuffer: wait for output buffer return timed out after 3000ms (max_buffers 2)
06-10 14:00:41.063 3150 4400 E Camera3-Device: RequestThread: Can't get output buffer, skipping request: Connection timed out (-110)
06-10 14:00:44.064 3150 4400 E Camera3-Stream: getBuffer: wait for output buffer return timed out after 3000ms (max_buffers 2)
06-10 14:00:44.064 3150 4400 E Camera3-Device: RequestThread: Can't get output buffer, skipping request: Connection timed out (-110)

**************************************************************************

Here's my question

1. Is there a patch to support UYVY(YUV422) cameras on Android9.0 ?

2.How to calculate and set the clock of MIPI CSI for 1920*1080P camera ?  The current default output Mipi Csi clock signal is 333M

Thanks!

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,251 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

 

1. supported sensors used in i.MX8M Mini EVK, formats can be found in driver

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/media/platform/mxc/capture/ov5640_...

2. one can look at below link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Setting-i-MX8M-Mini-and-Nano-MIPI-DPHY-C...

 

Best regards
igor

0 Kudos
Reply

1,233 Views
Andrew_yang
Contributor II

HI,igorpadykov

     Thanks for your replay,I still have some questions:

1.  Are there any reference examples support  YUV422 (UYVY)  sensors  formats in  android platform  HAL ?    as follow path:  Android9.0/vendor/nxp-opensource/imx/libcamera3

2. Question 2 introduces the clock calculation method of MIPI  DSI,I know this. but I want to know how to configure the clock of MIPI CSI ?

  • In the DTS file, I see that the clock of MIPI CIS default is set to 333M,  Whether this value can be modified directly ?   The camera output is 1080P.  What clock do I need to set ?

     " clock-frequency = <333000000>; "

***********************************************************

mipi_csi_1: mipi_csi@32e30000 {
compatible = "fsl,imx8mm-mipi-csi";
reg = <0x0 0x32e30000 0x0 0x1000>;
interrupts = <GIC_SPI 17 IRQ_TYPE_LEVEL_HIGH>;
clock-frequency = <333000000>;
clocks = <&clk IMX8MM_CLK_CSI1_CORE_DIV>,
<&clk IMX8MM_CLK_CSI1_PHY_REF_DIV>,
<&clk IMX8MM_CLK_DISP_AXI_ROOT>,
<&clk IMX8MM_CLK_DISP_APB_ROOT>;
clock-names = "mipi_clk", "phy_clk", "disp_axi", "disp_apb";
bus-width = <4>;
csi-gpr = <&dispmix_gpr>;
power-domains = <&mipi_pd>;
status = "disabled";
};

***********************************************************

Thanks !

0 Kudos
Reply