Xtal 24MHz oscillation i.MX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Xtal 24MHz oscillation i.MX6ULL

878件の閲覧回数
ban45
Contributor III

Hi

Does it oscillate when power is supplied to i.MX6ULL without writing a register?

Will oscillation stop if 3.3V is supplied to NVCC_PLL?

best regard

0 件の賞賛
3 返答(返信)

852件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

see below, please!

weidong_sun_0-1613294435151.png

Need to add a decoupling capacitor and a storage capacitor. Because this is the output of a power supply.

 

weidong

0 件の賞賛

872件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

>>Does it oscillate when power is supplied to i.MX6ULL without writing a register?
yes, it does.
No need for customer's software configuration, 24MHz can start the oscillation by itself.

>>Will oscillation stop if 3.3V is supplied to NVCC_PLL?
Yes, it will be possible.
NVCC_PLL is the output of the internal LDO_1P1, which supplies power to the internal PLL. If you connect 3.3V to this pin, the internal PLL will not work properly and may even damage the CPU. This is not allowed! It is entirely possible to cause the 24MHz crystal circuit to not work.

 

Have a nice day!

B.R,

Weidong

0 件の賞賛

864件の閲覧回数
ban45
Contributor III

Hi ,NXP TechSupport

What if I don't connect a capacitor?

What is the role of capacitors?

best regard

0 件の賞賛