Xtal 24MHz oscillation i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Xtal 24MHz oscillation i.MX6ULL

940 Views
ban45
Contributor III

Hi

Does it oscillate when power is supplied to i.MX6ULL without writing a register?

Will oscillation stop if 3.3V is supplied to NVCC_PLL?

best regard

0 Kudos
Reply
3 Replies

914 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

see below, please!

weidong_sun_0-1613294435151.png

Need to add a decoupling capacitor and a storage capacitor. Because this is the output of a power supply.

 

weidong

0 Kudos
Reply

934 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

>>Does it oscillate when power is supplied to i.MX6ULL without writing a register?
yes, it does.
No need for customer's software configuration, 24MHz can start the oscillation by itself.

>>Will oscillation stop if 3.3V is supplied to NVCC_PLL?
Yes, it will be possible.
NVCC_PLL is the output of the internal LDO_1P1, which supplies power to the internal PLL. If you connect 3.3V to this pin, the internal PLL will not work properly and may even damage the CPU. This is not allowed! It is entirely possible to cause the 24MHz crystal circuit to not work.

 

Have a nice day!

B.R,

Weidong

0 Kudos
Reply

926 Views
ban45
Contributor III

Hi ,NXP TechSupport

What if I don't connect a capacitor?

What is the role of capacitors?

best regard

0 Kudos
Reply