Hi All:
When I execute the gpu example(gpu_sdk_v1.00\Samples ,compiled success) ,Encountered an error:Xlib: extension "XFree86-DRI" missing on display ":0"
i has did some changes as the following:
> sudo ln -s libGAL-x11.so libGAL.so
> sudo ln -s libEGL-x11.so libEGL.so
> sudo ln -s libEGL-x11.so libEGL.so.1
> sudo ln -s libVIVANTE-x11.so libVIVANTE.so
libs of above was compiled use ltib
my board info: imx6q,bsp version is 3.0.35
what do i need to do next for the problem?
thanks!
as I known, ltib don't have x11 currently, you can move to yocto which has x11.
for how to download the yocto bsp, pls find it from official link.
<Embedded Linux for i.MX Applications Processors|NXP >.
focus on the "Board Support Packages" to download the bsp you need.