I'm using Yocto 2.1 system with X11 on imx6 platform.
XCB/OpenGL apps have various glitches in fullscreen mode, GUI components have a bad refresh, I think caused by performance (e.g in normal mode an application use 25 % CPU, in fullscreen use 71% and some times is blocked).
I think that OpenGL accelerator is stopped in fullscreen mode but i can't be sure.
UPDATE:
es2gears_x11 FAIL in fullscreen
glxgears OK
Hi Alessio
please try nxp demo images on
Also please check if used part has gpu (not all i.MX has it) and use attached Yocto Guide for image build and
Chapter 5 Graphics Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------