FlexCAN interface not working on i.MX 6SoloX M4 and A9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCAN interface not working on i.MX 6SoloX M4 and A9

1,599件の閲覧回数
bowenzhang
Contributor II

I have the same problem as below

FlexCAN interface not working on i.MX 6SoloX M4 and A9

but his answer is not right for me。

The FlexCAN library worked perfectly and I was able to perform many tests on a CAN network,however,when  I wanted to get the A9 to boot the M4 automatically when the power switch was turned on,flexcan  can not get/send  message。

jasonqueenjimtrudeauMandardhaval

ラベル(5)
0 件の賞賛
返信
4 返答(返信)

1,361件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Bowen,

Please look at the following thread. It is possible that A9 is reconfiguring clocks.

I.MX6 SoloX M4 Problem 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,361件の閲覧回数
bowenzhang
Contributor II

I have  reconfig clocks

0 件の賞賛
返信

1,361件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi bowen,

I assume you have solved this problem. If this is the case we would really appreciate if you could share how did you solved this issue.

Regards,

Carlos

0 件の賞賛
返信

1,361件の閲覧回数
bowenzhang
Contributor II

I have solved this problem,you can close this case for me and i will share myexperience later

0 件の賞賛
返信