X11 do not work on imx6dlsabred of yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

X11 do not work on imx6dlsabred of yocto

1,864 次查看
jiangyaqiang
Contributor V

HI :

    Could anyone help me for the problem of the topic ? 

    The XServer will crash on imx6dl , but it works on imx6q, with the same source and build config:

   release version: imx-4.1-krogoth(4.1.15-2.0.0)

  build config:

  for imx6q

   MACHINE=imx6qsabresd DISTRO=fsl-imx-x11 source ./fsl-setup-release.sh -b bld-x11

   bitbake fsl-image-qt5

  for imx6dl

  MACHINE=imx6dlsabresd DISTRO=fsl-imx-x11 source ./fsl-setup-release.sh -b bld-x11

   bitbake fsl-image-qt5

     Bellow is the log:

   

root@imx6dlsabresd:~# cat /var/log/Xorg.0.log
[2802098.994]
X.Org X Server 1.18.0
Release Date: 2015-11-09
[2802098.994] X Protocol Version 11, Revision 0
[2802098.994] Build Operating System: Linux 4.2.0-16-generic x86_64
[2802098.994] Current Operating System: Linux imx6dlsabresd 4.1.15+ #3 SMP PREEMPT Mon Jan 16 11:59:34 CST 2017 armv7l
[2802098.994] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 rootwait
[2802098.995] Build Date: 16 January 2017 06:06:22PM
[2802098.995]
[2802098.995] Current version of pixman: 0.32.8
[2802098.995] Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
[2802098.995] Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
[2802098.995] (==) Log file: "/var/log/Xorg.0.log", Time: Mon Jan 16 11:23:36 2017
[2802099.004] (==) Using config file: "/etc/X11/xorg.conf"
[2802099.005] (==) Using system config directory "/usr/share/X11/xorg.conf.d"
[2802099.011] (==) No Layout section. Using the first Screen section.
[2802099.011] (==) No screen section available. Using defaults.
[2802099.011] (**) |-->Screen "Default Screen Section" (0)
[2802099.011] (**) | |-->Monitor "<default monitor>"
[2802099.014] (==) No device specified for screen "Default Screen Section".
Using the first device section listed.
[2802099.014] (**) | |-->Device "i.MX Accelerated Framebuffer Device"
[2802099.014] (==) No monitor specified for screen "Default Screen Section".
Using a default monitor configuration.
[2802099.014] (**) Option "BlankTime" "0"
[2802099.014] (**) Option "StandbyTime" "0"
[2802099.014] (**) Option "SuspendTime" "0"
[2802099.014] (**) Option "OffTime" "0"
[2802099.014] (==) Automatically adding devices
[2802099.014] (==) Automatically enabling devices
[2802099.014] (==) Automatically adding GPU devices
[2802099.015] (==) Max clients allowed: 256, resource mask: 0x1fffff
[2802099.018] (WW) The directory "/usr/share/fonts/X11/misc/" does not exist.
[2802099.018] Entry deleted from font path.
[2802099.018] (WW) The directory "/usr/share/fonts/X11/TTF/" does not exist.
[2802099.018] Entry deleted from font path.
[2802099.018] (WW) The directory "/usr/share/fonts/X11/OTF/" does not exist.
[2802099.018] Entry deleted from font path.
[2802099.018] (WW) The directory "/usr/share/fonts/X11/Type1/" does not exist.
[2802099.018] Entry deleted from font path.
[2802099.018] (WW) The directory "/usr/share/fonts/X11/100dpi/" does not exist.
[2802099.018] Entry deleted from font path.
[2802099.018] (WW) The directory "/usr/share/fonts/X11/75dpi/" does not exist.
[2802099.018] Entry deleted from font path.
[2802099.018] (==) FontPath set to:

[2802099.018] (==) ModulePath set to "/usr/lib/xorg/modules"
[2802099.018] (II) The server relies on udev to provide the list of input devices.
If no devices become available, reconfigure udev or disable AutoAddDevices.
[2802099.020] (II) Loader magic: 0x1b1a58
[2802099.020] (II) Module ABI versions:
[2802099.020] X.Org ANSI C Emulation: 0.4
[2802099.020] X.Org Video Driver: 20.0
[2802099.020] X.Org XInput driver : 22.1
[2802099.020] X.Org Server Extension : 9.0
[2802099.022] (II) xfree86: Adding drm device (/dev/dri/card0)
[2802099.022] (II) no primary bus or device found
[2802099.022] falling back to /sys/devices/platform/Vivante GCCore/drm/card0
[2802099.022] (II) LoadModule: "glx"
[2802099.027] (II) Loading /usr/lib/xorg/modules/extensions/libglx.so
[2802099.071] (II) Module glx: vendor="X.Org Foundation"
[2802099.071] compiled for 1.18.0, module version = 1.0.0
[2802099.071] ABI class: X.Org Server Extension, version 9.0
[2802099.071] (==) AIGLX enabled
[2802099.071] (II) LoadModule: "vivante"
[2802099.072] (II) Loading /usr/lib/xorg/modules/drivers/vivante_drv.so
[2802099.078] (II) Module vivante: vendor="X.Org Foundation"
[2802099.078] compiled for 1.18.0, module version = 1.0.0
[2802099.078] Module class: X.Org Video Driver
[2802099.078] ABI class: X.Org Video Driver, version 20.0
[2802099.078] (II) VIVANTE: driver for vivante fb: VivanteGC500, VivanteGC2100,
VivanteGCCORE
[2802099.079] (--) using VT number 1

[2802099.179] (WW) Falling back to old probe method for vivante
[2802099.179] (II) Loading sub module "fbdevhw"
[2802099.179] (II) LoadModule: "fbdevhw"
[2802099.180] (II) Loading /usr/lib/xorg/modules/libfbdevhw.so
[2802099.181] (II) Module fbdevhw: vendor="X.Org Foundation"
[2802099.181] compiled for 1.18.0, module version = 0.0.2
[2802099.181] ABI class: X.Org Video Driver, version 20.0
[2802099.182] (II) VIVANTE(0): using default device
[2802099.182] (WW) VGA arbiter: cannot open kernel arbiter, no multi-card support
[2802099.182] (II) VIVANTE(0): Device preferred mode 'fb0':S:1920x1080p-60
[2802099.182] (II) VIVANTE(0): Creating default Display subsection in Screen section
"Default Screen Section" for depth/fbbpp 24/32
[2802099.183] (==) VIVANTE(0): Depth 24, (==) framebuffer bpp 32
[2802099.183] (==) VIVANTE(0): RGB weight 888
[2802099.183] (==) VIVANTE(0): Default visual is TrueColor
[2802099.183] (==) VIVANTE(0): Using gamma correction (1.0, 1.0, 1.0)
[2802099.183] (**) VIVANTE(0): Option "fbdev" "/dev/fb0"
[2802099.183] (II) VIVANTE(0): checking modes against framebuffer device...
[2802099.183] (II) VIVANTE(0): checking modes against monitor...
[2802099.183] (II) VIVANTE(0): Use built in mode (bpp 32)
[2802099.183] (--) VIVANTE(0): Virtual size is 0x0 (pitch 0)
[2802099.183] (==) VIVANTE(0): DPI set to (96, 96)
[2802099.183] (II) Loading sub module "fb"
[2802099.183] (II) LoadModule: "fb"
[2802099.183] (II) Loading /usr/lib/xorg/modules/libfb.so
[2802099.188] (II) Module fb: vendor="X.Org Foundation"
[2802099.188] compiled for 1.18.0, module version = 1.0.0
[2802099.188] ABI class: X.Org ANSI C Emulation, version 0.4
[2802099.188] (II) Loading sub module "exa"
[2802099.188] (II) LoadModule: "exa"
[2802099.188] (II) Loading /usr/lib/xorg/modules/libexa.so
[2802099.193] (II) Module exa: vendor="X.Org Foundation"
[2802099.193] compiled for 1.18.0, module version = 2.6.0
[2802099.193] ABI class: X.Org Video Driver, version 20.0
[2802099.346] (II) VIVANTE(0): printing discovered frame buffer 'fb0' supported modes:
[2802099.347] (II) VIVANTE(0): Modeline "S:1280x720p-50"x0.0 74.25 1280 1720 1760 1980 720 725 730 750 +hsync +vsync -csync (37.5 kHz e)
[2802099.347] (II) VIVANTE(0): Modeline "S:720x576p-50"x0.0 27.00 720 732 796 864 576 581 586 625 -hsync -vsync -csync (31.2 kHz e)
[2802099.347] (II) VIVANTE(0): Modeline "S:1920x1080p-50"x0.0 148.50 1920 2448 2492 2640 1080 1084 1089 1125 +hsync +vsync -csync (56.2 kHz e)
[2802099.348] (II) VIVANTE(0): Modeline "S:640x480p-60"x0.0 25.17 640 656 752 800 480 490 492 525 -hsync -vsync -csync (31.5 kHz e)
[2802099.348] (II) VIVANTE(0): Modeline "S:720x480p-60"x0.0 27.00 720 736 798 858 480 489 495 525 -hsync -vsync -csync (31.5 kHz e)
[2802099.348] (II) VIVANTE(0): Modeline "S:720x480p-60"x0.0 27.00 720 736 798 858 480 489 495 525 -hsync -vsync -csync (31.5 kHz e)
[2802099.348] (II) VIVANTE(0): Modeline "S:1280x720p-60"x0.0 74.25 1280 1390 1430 1650 720 725 730 750 +hsync +vsync -csync (45.0 kHz e)
[2802099.349] (II) VIVANTE(0): Modeline "S:1920x1080p-60"x0.0 148.50 1920 2008 2052 2200 1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)
[2802099.349] (II) VIVANTE(0): Modeline "V:640x480p-60"x0.0 25.20 640 656 752 800 480 490 492 525 -hsync -vsync -csync (31.5 kHz e)
[2802099.349] (II) VIVANTE(0): Modeline "D:1920x1080p-60"x0.0 148.50 1920 2008 2052 2200 1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz e)
[2802099.349] (II) VIVANTE(0): Modeline "V:640x480p-60"x0.0 25.20 640 656 752 800 480 490 492 525 -hsync -vsync -csync (31.5 kHz e)
[2802099.392] (II) VIVANTE(0): Output DISP3 BG has no monitor section
[2802099.392] (II) VIVANTE(0): Printing probed modes for output DISP3 BG
[2802099.392] (II) VIVANTE(0): Modeline "S:1920x1080p-60"x60.0 148.50 1920 2008 2052 2200 1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)
[2802099.392] (II) VIVANTE(0): Modeline "S:1920x1080p-50"x50.0 148.50 1920 2448 2492 2640 1080 1084 1089 1125 +hsync +vsync -csync (56.2 kHz e)
[2802099.392] (II) VIVANTE(0): Modeline "S:1280x720p-50"x50.0 74.25 1280 1720 1760 1980 720 725 730 750 +hsync +vsync -csync (37.5 kHz e)
[2802099.392] (II) VIVANTE(0): Modeline "S:1280x720p-60"x60.0 74.25 1280 1390 1430 1650 720 725 730 750 +hsync +vsync -csync (45.0 kHz e)
[2802099.392] (II) VIVANTE(0): Modeline "S:720x576p-50"x50.0 27.00 720 732 796 864 576 581 586 625 -hsync -vsync -csync (31.2 kHz e)
[2802099.392] (II) VIVANTE(0): Modeline "S:720x480p-60"x59.9 27.00 720 736 798 858 480 489 495 525 -hsync -vsync -csync (31.5 kHz e)
[2802099.392] (II) VIVANTE(0): Modeline "V:640x480p-60"x60.0 25.20 640 656 752 800 480 490 492 525 -hsync -vsync -csync (31.5 kHz e)
[2802099.392] (II) VIVANTE(0): Modeline "S:640x480p-60"x59.9 25.17 640 656 752 800 480 490 492 525 -hsync -vsync -csync (31.5 kHz e)
[2802099.393] (II) VIVANTE(0): Output DISP3 BG connected
[2802099.393] (II) VIVANTE(0): Using exact sizes for initial modes
[2802099.393] (II) VIVANTE(0): Output DISP3 BG using initial mode S:1920x1080p-60 +0+0
[2802099.393] (II) VIVANTE(0): imxDisplayPreInit: virtual set 1920 x 1080, display width 0
[2802099.393] (II) VIVANTE(0): FBDevPreInit: adjust display width 1920
[2802099.393] (**) VIVANTE(0): PreInit done
[2802099.393] (--) Depth 24 pixmap format is 32 bpp
[2802099.393] (II) VIVANTE(0): Init mode for fb device
[2802099.917] (II) VIVANTE(0): hardware: DISP3 BG (video memory: 16335kB)
[2802099.918] (II) VIVANTE(0): FB Start = 0x7558d000 FB Base = 0x7558d000 FB Offset = (nil) FB PhyBase 0x3cc00000
[2802099.918] (II) VIVANTE(0): reserve 8355840 bytes for on screen frame buffer; total fb memory size 16727040 bytes; offset of shadow buffer 8355840
[2802099.963] (II) VIVANTE(0): hardware: DISP3 BG (video memory: 16335kB)
[2802099.977] (II) VIVANTE(0): test Initializing EXA
[2802099.980] (EE)
[2802099.980] (EE) Backtrace:
[2802099.980] (EE)
[2802099.980] (EE) Segmentation fault at address 0xc
[2802099.980] (EE)
Fatal server error:
[2802099.980] (EE) Caught signal 11 (Segmentation fault). Server aborting
[2802099.981] (EE)
[2802099.981] (EE)
Please consult the The X.Org Foundation support
at http://wiki.x.org
for help.
[2802099.981] (EE) Please also check the log file at "/var/log/Xorg.0.log" for additional information.
[2802099.981] (EE)
[2802100.050] (EE) Server terminated with error (1). Closing log file.

标记 (1)
0 项奖励
回复
1 回复

991 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Please check solution provided in x-server seg faults in iMX6Q Custom board. and let us know if this works for your case. or follow up: https://community.nxp.com/thread/443206 

0 项奖励
回复