Wince 7 Booting Issue in sabre board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wince 7 Booting Issue in sabre board

3,839 Views
bipulpandey
Contributor II

HI,

I am trying to boot  WINCE7 my SABRE (SDP)Platform (I.MX 6). I have download the binary (iMX6Q_SABRE_SD_WEC7_v3.1.1.10_bin) for WEC7  from

http://www.adeneo-embedded.com/Products/Board-Support-Packages/Freescale-i.MX6

I found the folders

1-      Tool :  where I got the Cfimager and read me file

2-      Binaries\multimedia

Eboot.nb0 

Nk.bin

Nk.nb0

Then I follow the steps  that is written in the readme.txt  I formatted the SD card

I flash the eboot.nb0 and nk.nb0 through the cmd

cfimager -f eboot.nb -d f  -e nk.nb0  –a  (f is drive name where SD card is inserted).

It is completed and says done! 100%

Then I have inserted the card to hardware (sabre board) nothing is coming out through screen . I also not receive any data from serial port

Please help me on that

Thanks

Bipul pandey 

Labels (1)
Tags (3)
0 Kudos
Reply
11 Replies

3,045 Views
SergioSolis
NXP Employee
NXP Employee

I haven't tried to flash the board with WinCE7 but I'm not sure if you are setting the board's dip-switch setting to "2" and "7" so the board knows it has to boot from the SD Card.

AdeneoEmbedded  do you have any information that might help?


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,045 Views
bipulpandey
Contributor II

Hi Sergio,

Yes I have set "2" and "7". And not able to see anything on the board. as the image of android that came by default in SD card Boots properly. after that i follow

the steps that i have mentioned .

Thanks

Bipul Pandey

0 Kudos
Reply

3,045 Views
SergioSolis
NXP Employee
NXP Employee

Thank you for your prompt response!, 

Vipul, were you able to make it work with the suggestion from Adeneo?

0 Kudos
Reply

3,045 Views
bipulpandey
Contributor II

Hi Sergio,

As still we are not able to UP the board so please help me on that. 

Regards,

Bipul Pandey

0 Kudos
Reply

3,045 Views
bipulpandey
Contributor II

Hi,

The CMD that Adeneo Support Team support suggested  not working . i have tried but the result is same nothing is coming out through display .and same at com port

The things that I have done, I format the card as FAT32 by window machine then fire the cmd that suggested by the adeneo

below is the screen shot of cmd, here every thing looks very fine

ResultFromCmd.png

after that i inserted the card  into board,"nothing is happening " .then i inserted the card that boot the android , system boots properly i have seen the message at com port.(DIP Switch setting SW6 "2"and "7" set at booth case)

i want to know one thing.

1- first the boot loader run at the location 0x2 (are there any debug message came out when boot loader runs ?) if debug message are there that means boot loader is not running (i have not seen any message at com port)


please help me on that what to do next.


Regards

bipul pandey

0 Kudos
Reply

3,045 Views
bipulpandey
Contributor II

Hi Team,

Have you got something Please solve the issue , I am waiting your reply

or is there any one who can help on that

@Sergio  Do you have any point here ...

Regards,

Bipul Pandey

0 Kudos
Reply

3,045 Views
SergioSolis
NXP Employee
NXP Employee

I'm sorry Bipul, since WinCE is not developed by Freescale there isn't much I could know about it, besides I haven't actually installed WinCE in the i.MX6 board.  Deactivated user developed this BSP, they are the team that has the experience with it.

0 Kudos
Reply

3,045 Views
bipulpandey
Contributor II

Hi Team,

As i have tried your option here but no Luck :-(

1- I have change the SD card

2- check with the SW6 switch setting

3- the CheckSum of all image is correct

As now i have tried so many thing as you suggested . i have point here

1- There is no problem Of SD card slot, SD card is attaching properly (as android is booting).

3- No DIP Switch setting Issue.

2- No problem with Images (as all the check sum are correct)

Now the doubt on SD card partition and flashing the image on SD card.

So please think on that side and let me know please

1-how to verify that image and boot loader on the SD card flash properly(I have doubt only here)

2- how many partition SD card create when be it formatted by -a CMD and when files are copied

Please solve the issue on high priority

We have two board and no of use right now.

if possible please arrange the call or webex meeting.

Thanks

Bipul Pandey

0 Kudos
Reply

3,045 Views
bipulpandey
Contributor II

Hi Team

1- I tried with new SD card so there is no point here for using enough time

2- I also used to reset the board with SW2 and for info (android is booting)

3- I check the partition of SD card and I have found, There is no data at 400 ,80400,8080400  Location ,I will share the snapshot also, So problem is here in the SD card .It is not flashed correctly by your cmd . so please correct that or send new procedure to flash the image to up the board

And i found the data in android SD card.

P1.jpg

P2.jpg

p3.jpg

Regards,

Bipul Pandey

0 Kudos
Reply

3,045 Views
bipulpandey
Contributor II

Sticker label near to power socket is MCIMX6DL-SDP

sticker near to SW6 is SCH-27417 REV C4  second sticker 700-27417 REV C

0 Kudos
Reply

3,045 Views
bipulpandey
Contributor II

Hi,

I have not try the option that you have told,i will try it tomorrow

any way I want to know

how is the partition done by the the cfimager -d f -f nk.nb0 -imx53 -a CMD ? , what is the partition name because i have not seen any partition after firing the CMD.


Thanks

Bipul Pandey

 

0 Kudos
Reply