Will we have new BSP for i.MX6 Android 4.4(or above) which helps support USB Bluetooth dongle?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Will we have new BSP for i.MX6 Android 4.4(or above) which helps support USB Bluetooth dongle?

1,608 次查看
robrob
Contributor I

We are trying to porting product into Android Kitkat, but we got a problem.

Bluetooth stack is changed to BlueDroid, but it only support uart interface communication.

Does we will have more support on USB Bluetooth dongle in latest Android?

标签 (2)
0 项奖励
回复
4 回复数

981 次查看
mutyalaraoneela
Contributor III

Hi all,

  I am glad to inform you that the above issue which I have posted earlier got resolved, but I have another 2 issues one while data transfer, the other while enabling via GUI.

   1) After enabling bluetooth, while transferring file from third party mobile to IMX_6SL board, file is getting transferred(TX), but vice versa (RX) is not happening, it is giving the error message :

   File not Received

   File : sample.jpg

   Reason : Storage issue

  2) And presently I am inserting my driver via GUI, I am getting an error message while enabling bluetooth via GUI   ie Operation not permitted while loading .ko (driver)Please suggest me what to do?? whether I need to install my driver at boot by adding in init.rc?? if I do it always on boot bt will be in ON State only??  OR Do i need to build my driver along with android source code???

Please suggest me how to proceed further???

Thanks and Regards,

Mutyala Rao.

0 项奖励
回复

981 次查看
igorpadykov
NXP Employee
NXP Employee

Hi rob

as far as I know new KK443 will have the same BT

connectivity.

Best regards

igor

981 次查看
robrob
Contributor I

Dear Igor,

So glad to hear that!

Thanks for your kindly reply!

(update) Just one more question:

Is Android 443 BSP will be released soon? supposed when will it be available?

Best regards,

rob

0 项奖励
回复

981 次查看
igorpadykov
NXP Employee
NXP Employee

Hi rob

it is planned on Feb-2015

Best regards

igor