Will any GPIO interrupt wake-up the iMX6DL from deep sleep?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Will any GPIO interrupt wake-up the iMX6DL from deep sleep?

494 次查看
ismaeltorres
Contributor I

I see in the documentation that while the iMX6DL is in deep sleep, only keypad, GPIO, and SNVS will wake it up. But the question is if any of the GPIO interrupts is wake up capable or only some of them, like those listed as GPIO1 0-7 / INT0-7.

Thanks.

Ismael.

标签 (1)
0 项奖励
回复
1 回复

399 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ismael

yes any GPIO interrupt is capable to wake up

from low power modes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复