Who should I contact for technical questions for the TFT3P5581-E MIPI Display recommended with the i.MX7 Sabre Board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Who should I contact for technical questions for the TFT3P5581-E MIPI Display recommended with the i.MX7 Sabre Board?

1,687件の閲覧回数
johnathanfeuers
Contributor II

I would like technical information for the TFT3P5581-E MIPI Display recommended here: 

https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fwebapp%2Fsearch...

Where can I find the supplier / datasheet / etc...?

Thanks.

ラベル(2)
4 返答(返信)

1,118件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Johnathan Feuerstein,

There is no technical information on the NXP website but the manufacturer is Truly Semiconductor. I hope this help you find the datasheet and further technical information.

Regards,

1,118件の閲覧回数
johnathanfeuers
Contributor II

Hello,

Thank you for the reply! The manufacturer information was helpful, I was able to get in contact with TRULY to discuss.

FYI this display is a custom part, and so they were not able to provide me technical information directly. I was informed that other customers cannot buy these custom parts without 'authorization'.

But they are able to recommend other display options so I should be able to find another solution. Thanks for the help.

Regards,

John

0 件の賞賛
返信

1,117件の閲覧回数
sinanakman
Senior Contributor III

Hi Johnathan, would you be able to share what other display options they recommended to you. This would be of interest.

Thanks and best regards.

Sinan Akman

0 件の賞賛
返信

1,118件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Johnathan Feuerstein,

Perhaps the following thread may be of help. This display can be connected to the MX7 Sabre board directly and the thread follows a bit of the configuration although it does not provide the datasheet.

https://community.nxp.com/thread/443466

I hope this helps!

Regards

0 件の賞賛
返信