Which file should I download?IMX6X4EVM10ABCTAD1533-6SX SABRE-SDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which file should I download?IMX6X4EVM10ABCTAD1533-6SX SABRE-SDB

401 次查看
guojqf
Contributor I

I originally downloaded this,but I meet a lot of problem!

guojqf_0-1620975724359.png

guojqf_1-1620975778166.png

My development board is IMX6X4EVM10ABCTAD1533-6SX SABRE-SDB(NXP)

I don't know if I downloaded the file by mistake,and flash a 

I also refer to the IMX linux users guide,but useless.

if I copy the full SD card image,it is no problem.but when I read 4.3.3 ->4.3.6,I meet a lot of problem.

I don't know if I downloaded the file by mistake, and flash the useless file to my board.

 

So,my board is IMX6X4EVM10ABCTAD1533-6SX SABRE-SDB,which file should I flash to my board?!

guojqf_2-1620975912325.png

 

 

0 项奖励
回复
0 回复数