I have read below link but can not find board/freescale/mx6q_sabresd/flash_header.S.
Futhermore other files in most of documents are not exist, it is concerned with old BSP, I think.
How to Create i.MX6 32bit DDR3 Script Based on 64bit DDR3 Script
Where is updated documents about 32bit DDR3 Script for 3.10.53 BSP?
已解决! 转到解答。
ddr configured in *.cfg files, like uboot../board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg
so one needs to modify it for 32bit memory configuration
Hi JHY
32bit memory configuration is supported in FSL 3.10.53 BSP
refer to attached Linux Guide sect.5 "Enabling Solo Emulation"
included in L3.10.53_1.1.0_LINUX_DOCS
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------