Where is the demo for Two-Way Video

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the demo for Two-Way Video

ソリューションへジャンプ
1,275件の閲覧回数
ivyliu
Contributor IV

Hi All,

In IMX6 Quad/Dual Application Processor Reference Manual (IMX6DQRM.pdf), chapter 9, Table 9-1 Video/graphics applications, there mentioned a Two-way Video application.

Does anyone know how can I find the source code for this application?

Thanks and Best Regards,

Ivy

ラベル(5)
0 件の賞賛
返信
1 解決策
1,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

seems this use case is described on p.4 presentation as "Full-Duplex" use case

Q&A: MX6 VPU H.264 Dual Stream Encode Limits 

for sources one can look at units test (imx-test/..mxc_vpu_test, check

documentation FSL-UT-VPU-007.txt for Decode and encode simultaneously)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

Also Table 9-1 just described use cases where porcessor may be used,

not fully developed demo with ready sources. So imx-test may be used just as

starting point for developing such demo.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,127件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

seems this use case is described on p.4 presentation as "Full-Duplex" use case

Q&A: MX6 VPU H.264 Dual Stream Encode Limits 

for sources one can look at units test (imx-test/..mxc_vpu_test, check

documentation FSL-UT-VPU-007.txt for Decode and encode simultaneously)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

Also Table 9-1 just described use cases where porcessor may be used,

not fully developed demo with ready sources. So imx-test may be used just as

starting point for developing such demo.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,126件の閲覧回数
ivyliu
Contributor IV

Hi Igor,

Thank you very much!

Best Regards,

Ivy

0 件の賞賛
返信