Hi all
I'm using i.MX6Solo and have questions about uSDHC controller.
According to Figure 67-2 of RM, Async FIFO use a clock that selected from CLK(input) or CLK(output).
Where CLK(input) come from ?
And how can user select CLK(input) or CLK(output) ?
ko-hey
已解决! 转到解答。
Hello,
Terms CLK, DATA[7:0], and CMD relate to SD interface. In this sense
the CLK(input) is not used on i.MX6 uSDHC. CLK(output) is SD clock,
please refer to section 67.4.5 (Clock Generator) of the RM how it is generated.
Also, the base clock is the peripheral clock ipg_clk (from ipg_clk_root), mentioned
in Table 67-5 (uSDHC Clocks) of the RM.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Terms CLK, DATA[7:0], and CMD relate to SD interface. In this sense
the CLK(input) is not used on i.MX6 uSDHC. CLK(output) is SD clock,
please refer to section 67.4.5 (Clock Generator) of the RM how it is generated.
Also, the base clock is the peripheral clock ipg_clk (from ipg_clk_root), mentioned
in Table 67-5 (uSDHC Clocks) of the RM.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------