What is the maximum input voltage for VLDO34, in MC32PF3000A2EP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the maximum input voltage for VLDO34, in MC32PF3000A2EP?

550件の閲覧回数
logeshs
Contributor II

In reference to What is the maximum input voltage for VLDO34, in MC32PF3000A2EP  

Currently we have connected as per Warp reference design. In Warp design, you have connected PMIC_PWR to VLDO34IN. Also, PMIC_PWR is ORed with VBAT. In this case PMIC_PWR will get >3.6V at full charge right? Will this damage the PMIC pin? Should we follow the datasheet or the reference design? Please refer the Warp schematic.

Thank you

ラベル(1)
0 件の賞賛
返信
1 返信

426件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Logesh

it is necessary to follow the datasheet. Please note that sometimes

designs are developed when datasheets are not fully validated using some

preliminary data.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信