AnsweredAssumed Answered

What is the maximum input voltage for VLDO34, in MC32PF3000A2EP

Question asked by Logesh S on Dec 19, 2017
Latest reply on Jan 23, 2018 by marcfigliuolo

Hi,

We are using PMIC MC32PF3000A2EP in our design with MCIMX7D3EVK10SD.

 

1: What is the maximum input voltage for VLDO34? There are two different specs available in datasheet. At page 25, it shows 2.8V to 3.6V. In Figure 5 Power map, VLDO4 input is connected to VIN and says 4.5V(Typ).

 

Please let us know which one should I refer.

 

Thanks

Logesh

Outcomes