What is the maximum SPI slave devices supported by SPI controller in i.mx8MM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the maximum SPI slave devices supported by SPI controller in i.mx8MM?

423件の閲覧回数
richard_hu
Contributor V

Hi, Sir:

We have a require to enable 8 SPI slave devices on ECSPI2 of i.mx8MM.(using GPIO chip selects)

But we see the description in i.mx8mm TRM denotes the SPI controller supports 4 chip selects for  maximum.

screenshot_1_1632463733.png

 

If we use GPIO chip selects instead of native chip select, does it still limit to four SPI devices?

Or it can support more than four SPI devices?

 

Thanks~!

BR,

 

Richard 

 

 

0 件の賞賛
1 返信

411件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Richard

 

>If we use GPIO chip selects instead of native chip select, does it still limit to four SPI devices?

 

no, in case of GPIO chip selects it is not limited.

 

Best regards
igor

0 件の賞賛