Hi All,
I want to know the version of ath6kl driver in Marshmallow. I tried flashing Marshmallow on SD card but i could not do it. But that is another issue about which i am not worried right now. My target was to flash SD card with Marshmallow and check ath6kl version which shows at boot time.
Best Regards,
Hare
解決済! 解決策の投稿を見る。
Hi Hare
Marshmallow uses Broadcom drivers as shown
in attached Table 2. Features Release Notes.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I do not know what is "android release (eng-L5.0.2_1.0.0-ga)",
attached documents are for nxp official releases (found on nxp.com) :
L5.0.0_1.0.0-ga, also Android L5.1.1_2.1.0 uses broadcom BCM4339
as shown in attached Release Notes p.4
Suggest to look at document Release Notes - it should be included in bsp,
it shows what is supported. Note, there may be other drivers, but they are not
supported (tested).
~igor
igor,
In imx android release (eng-L5.0.2_1.0.0-ga), there is atheros driver in hardware/imx/wlan/atheros/ location which is getting used ... and there will be another driver which is the part of linux kernel itself.(kernel_imx/drivers/net/wireless/ath/). What is the difference between these two version. And as we see, the one which is hardware/imx folder is getting used .
-Shiva
Hi igor,
There is another question in this context.
Lolypop usage atheros driver . And in the same kernel version on linux i have found different architecture of atheros driver.
Could you please explain me why this difference is there??
Thank you igor for your valuable answer.
Best Regards,
Hare
Hi Hare
Marshmallow uses Broadcom drivers as shown
in attached Table 2. Features Release Notes.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------