What is the ath6kl driver version in Marshmallow?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the ath6kl driver version in Marshmallow?

Jump to solution
1,370 Views
harekrishnaroy
Contributor III

Hi All,

I want to know the version of ath6kl driver in Marshmallow. I tried flashing Marshmallow on SD card but i could not do it. But that is another issue about which i am not worried right now.  My target was to flash SD card with Marshmallow and check ath6kl version which shows at boot time.

Best Regards,

Hare

Labels (2)
1 Solution
1,148 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hare

Marshmallow uses Broadcom drivers as shown

in attached Table 2. Features Release Notes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
6 Replies
1,148 Views
igorpadykov
NXP Employee
NXP Employee

I do not know what is "android release (eng-L5.0.2_1.0.0-ga)",

attached documents are for nxp official releases (found on nxp.com) :

L5.0.0_1.0.0-ga, also Android L5.1.1_2.1.0 uses broadcom BCM4339

as shown in attached Release Notes p.4

Suggest to look at document Release Notes - it should be included in bsp,

it shows what is supported. Note, there may be other drivers, but they are not

supported (tested).

~igor

0 Kudos
1,148 Views
shivakumar
Contributor II

igor,

In imx android release (eng-L5.0.2_1.0.0-ga), there is atheros driver in hardware/imx/wlan/atheros/ location which is getting used ... and there will be another driver which is the part of linux kernel itself.(kernel_imx/drivers/net/wireless/ath/). What is the difference between these two version. And as we see, the one which is hardware/imx folder is getting used .

-Shiva

1,148 Views
igorpadykov
NXP Employee
NXP Employee

as shown in attached Release Notes Android supports 8821AS, Linux AR6003

~igor

0 Kudos
1,148 Views
harekrishnaroy
Contributor III

Hi igor,

There is another question in this context.

Lolypop usage atheros driver .  And in the same kernel version on linux i have found different architecture of atheros driver.

Could you please explain me why this difference is there??

0 Kudos
1,148 Views
harekrishnaroy
Contributor III

Thank you igor for your valuable answer.

Best Regards,

Hare

0 Kudos
1,149 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hare

Marshmallow uses Broadcom drivers as shown

in attached Table 2. Features Release Notes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos