Hi all,
I am trying to enable watchdog in u-boot for imx6. I am using Yocto - imx_v2016.03_4.1.15_2.0.0_ga in SABRESD board.
In uboot .bb file i addedfollwing lines,
FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}-${PV}:"
SRC_URI += "file://watchdog.patch"
SRC_URI += "file://watchdog1.patch"
In these 2 patches, the below changes are done.
path : git/include/configs$ vim mx6sabresd.h
/* Enabled Watchdog Timer */
#define CONFIG_IMX_WATCHDOG
In another patch, I reduced the restarting time in
#define CONFIG_WATCHDOG_TIMEOUT_MSECS 6000
Then i cleaned and compiled the u-boot. My patches are applied in source but the board is not restarting. Can anyone help me to enable the Watchdog.
解決済! 解決策の投稿を見る。
I have got solution for my problem. I successfully enabled watchdog in u-boot.
With the addition of my question i have called the hw*_init() in board related file. This action will initialize that watchdog HW functions. Thank you.
I have got solution for my problem. I successfully enabled watchdog in u-boot.
With the addition of my question i have called the hw*_init() in board related file. This action will initialize that watchdog HW functions. Thank you.
Hi Karthikeyan
watchdog is not used in nxp uboot
uboot-imx.git - Freescale i.MX u-boot Tree
however one can try to debug it checking watchdog registers with
sect.70.7.1 Watchdog Control Register (WDOGx_WCR) i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
Note, for reliable reset watchdog should reset power for whole board, not only for
i.MX6 processor. For example check MMPF0100 PWRON and WDOG connection on
SabreSD board spf-27392 schematic p.21
Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------