Wandboard Quad: how to use hw decoding video playback?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wandboard Quad: how to use hw decoding video playback?

1,093 次查看
abhayghatpande
Contributor III

Hello I'm using the dizzy branch and built Chromium using the meta-browser repository. chrome://gpu reports:

Graphics Feature Status

Canvas: Hardware accelerated

Flash: Hardware accelerated

Flash Stage3D: Hardware accelerated

Flash Stage3D Baseline profile: Hardware accelerated

Compositing: Hardware accelerated

Rasterization: Hardware accelerated

Threaded Rasterization: Enabled

Video Decode: Hardware accelerated

Video Encode: Hardware accelerated

WebGL: Hardware accelerated

But when I try to play an mp4 video, it lags severely, doesn't seem to be using hw decoding. I just open the file on disk using file:// URI.

What could be the reason? gstreamer plays the same video smoothly. How to play the same video in Chromium hw accelerated?

0 项奖励
回复
2 回复数

737 次查看
abhayghatpande
Contributor III

Is it possible for someone to confirm if Chromium supports VPU-accelerated MP4 decoding on i.MX6Q?

If this is something that is not currently feasible, then I will redirect my efforts to other pending issues.

Will appreciate all inputs. Thanks,

0 项奖励
回复

737 次查看
abhayghatpande
Contributor III

The same video with Webm plays hardware accelerated without problems. I'm guessing this has something to do with the libavcodec and libh264 warnings I had when I built Chromium.

0 项奖励
回复