Video Capture Latency I.MX6_MAX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Video Capture Latency I.MX6_MAX

1,895 Views
rajvikamdar
Contributor III

Hi All

 We are trying to capture video over nitrogen_6max board. We are using ov5640 camera module and OS as Android Kitkat.

- With the setup as explained above, we are getting capture video latency of about 150ms. We need to reduce this latency to 30ms. Our commercial production is at stake.

Can you guys help me where to debug onto, is the latency due to Android Framework or HAL or ov5640 camera driver.

Since the camera architecture is huge, we are unable to pin point on the particular section..

Your help is highly appreciated.

Regards

Rajvi

Labels (4)
0 Kudos
Reply
2 Replies

1,741 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Kamdar,

This link going to be helpfull:

https://community.nxp.com/thread/308415 

0 Kudos
Reply

1,741 Views
rajvikamdar
Contributor III

Thank you for replying.

Actually we are using 2 nitrogen6_max board. 1 as miracast source and another as miracast sink.

We are not using software decoder.

Hence the link that you suggested would not be of help for us. If you could guide us more on hardware decoder/encoder or miracast source/sink would be great.

Our production is at stake. Requesting a help on urgent basis.

Thanks

Rajvi

Sent from my iPhone

0 Kudos
Reply